N Kanbe I9

  • Total activity 7
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 2

Posts

Recent activity by N Kanbe I9 Recent activity Votes
  • D455-How can I see far away

    Hello I'm using D455, but I can't measure far.How can I measure far? I installed the D455 and gradually lowered the person to see how far I could measure.As a result, I could only see up to 3.9m. B...

  • How to calibrate L515

    Hello I am currently using L515. When using L515, the maximum distance error is about 20 cm. The distance from the camera in the green part of the attached image is about 1 m, and the dark red is ...

  • [L515]Is it possible to match alignment of color image and depth image?

    I'm currently using the L515 with NVIDIA's Jetson NX.In the process I do, I need to match the alignment in the color and depth images. (process)1, Detect a person in a color image and get the coord...