N Kanbe I9
- Total activity 7
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Activity overview
Latest activity by N Kanbe I9-
N Kanbe I9 created a post,
D455-How can I see far away
Hello I'm using D455, but I can't measure far.How can I measure far? I installed the D455 and gradually lowered the person to see how far I could measure.As a result, I could only see up to 3.9m. B...
-
N Kanbe I9 commented,
Thank you very much. My question has been resolved.
-
N Kanbe I9 commented,
Thank you very much. Since the range of color images is narrow, we will consider other methods.
-
N Kanbe I9 created a post,
How to calibrate L515
Hello I am currently using L515. When using L515, the maximum distance error is about 20 cm. The distance from the camera in the green part of the attached image is about 1 m, and the dark red is ...
-
N Kanbe I9 created a post,
[L515]Is it possible to match alignment of color image and depth image?
I'm currently using the L515 with NVIDIA's Jetson NX.In the process I do, I need to match the alignment in the color and depth images. (process)1, Detect a person in a color image and get the coord...