Bbiehler
- Total activity 5
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Comments
Recent activity by Bbiehler-
Still no success. I started with the medium density presets, adjusted the exposure time and turned the laser power to its maximum, but did not see improvements: The red arrow points to the left wa...
-
So I changed the setup a bit: Distance to the objekt is now 0.1 m, resolution 848x480, and I worked with the disparity shift in the range of 40 to 150. The Depth units are 0.0001.Still the Post-Pr...
-
Yes, I can confirm that it is this U-shaped object. For a better understanding there is another picture of the extruded profile as seen from diagonally above and the part zoomed in from the other p...