Bbiehler

  • Total activity 5
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Bbiehler
  • Bbiehler commented,

    Still no success. I started with the medium density presets, adjusted the exposure time and turned the laser power to its maximum, but did not see improvements: The red arrow points to the left wa...

  • Bbiehler commented,

    So I changed the setup a bit: Distance to the objekt is now 0.1 m, resolution 848x480,  and I worked with the disparity shift in the range of 40 to 150. The Depth units are 0.0001.Still the Post-Pr...

  • Bbiehler commented,

    Yes, I can confirm that it is this U-shaped object. For a better understanding there is another picture of the extruded profile as seen from diagonally above and the part zoomed in from the other p...

  • Bbiehler created a post,

    D435 won't detect small walls

    I'm trying to detect aluminum profiles seen from the front side, as seen in the image below. I used the Threshold Filter to get rid of the background, played with the exposure and auto exposure an...