Cor2
- Total activity 14
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 5
Activity overview
Latest activity by Cor2-
Cor2 commented,
In most (if not all) VR headsets, the optical tracking is combined with the accelaration sensor and gyroscoop information. This sensor fusion will fail if you use this system inside a moving cabin,...
-
Cor2 commented,
I'm affraid I will need their support in my situation. The thing is that I would like to use it inside a moving cabine. So I want to disable the gyroscope and acceleration sensor.Maybe you (Euh219)...
-
Cor2 created a post,
How to track VR headset in a moving cabin
Hi,We have a problem. We need to track a VR headset inside a moving cabin. The optical tracking that comes with the headset can therefore not be used.So I'm searching for an alternative. Could I us...
-
Cor2 created a post,
T265 for VR headset tracking
I need to track a VR headset. The optical tracking that comes with the headset can not be used because the headset is used inside a moving cabin.Can I mount a T265 on the headset to track its posit...
-
Cor2 created a post,
Should I avoid the T265 for new projects?
Hi,I'm investigating the use of RealSense cameras for my project. This includes the T265. But when I read the last posts on this forum about the T265, it seems that support for T265 is dead.Is this...
-
Cor2 commented,
Hello Marty, thx for fast reaction again.About this high speed capture mode: Can we program the offset of these 100 lines? We need to 'follow' the target by defining which part of the image to stre...
-
Cor2 created a post,
Can we connect D435 to a Jetson Nano or Jetson Xavier board?
We really would like to connect (multiple) D435 units to a Jetson Nano or Jetson Xavier board. Can the SDK be installed on these boards? Anyone experience with this?If not possible, Is there a work...
-
Cor2 commented,
Thx for the quick answer!The reason I would like to stream only part of the image is bandwidth limitation. We want to connect multiple D435 units to the same computer. And also because we would lik...
-
Cor2 created a post,
D435: Can I stream part of the IR or RGB pictures?
Hi, I'm new to the RealSense camera. We are investigating if we can use the D435 for some special tracking.We would like to know if we can stream only part of the left/right IR image and/or RGB ima...