Yixun Liu
- Total activity 154
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 53
Comments
Recent activity by Yixun Liu-
If I change the index from 1 to -1 it works.
-
On Android with Java the following code generate exception: Failed to start pipeline. Couldn't resolve requests. config.enableStream(StreamType.INFRARED, 1, 640, 480, StreamFormat.RGB8, 30); ...
-
If I use the 'RGB from left infrared' mode of the D405 when I do OpenGL rendering I need to use the intrinsic of the depth or the infrared 1 intrinsic, right?
-
Thank you so much for your quick response.
-
It looks this API is different from the Java API shipped with RealSense SDK. It does provide the interface I need but lacks documentation and examples. Can I used it along with the Java API shipped...
-
The room temperature is stable. I do not know how the temperature change because I did not touch the camera. Does the RealSense SDK has an API to monitor the camera temperature? My algorithm only ...
-
I am sorry. I gave you wrong answer regarding the question about how to install the SDK. Actually I built it from the source code. I know the command to check the FW version, but how to know the SD...
-
I installed the SDK with the installer program, but it is an old version installed several years ago. Do I need to install the latest? If yes, uninstall the old one first and then install the latest?
-
The following pic shows the error with the D455 camera not detected.
-
BTW, for the D455 which can be detected correctly and also can stream in RealSense Viewer, as I run the command as you said I got the following. What the meaning "malformed vid string..."?