Running D455 for long time and looks not stable
Hi,
I have a D455 camera and I use both left and right infrared cameras to do stereo matching.
The camera run 2 hours and works well by successfully matching both left and right subpixel features in a fixed scene. But after running 2 hours the matching is not stable. The lighting condition was fixed and the scene also did not change. The only reason we can guess is the image quality might be unstable after a long time running.
I want to know if my guess is true and how to verify it?
Thanks.
Yixun
-
Hi Yixun Liu Is the temperature in the room or the temperature of the camera liable to change over the course of two hours? The D455 camera model has a thermal compensation feature that can amend the depth value based on current temperature.
You can test in the RealSense Viewer tool whether thermal compensation is responsible by going to the Stereo Module > Controls section of the Viewer's options side-panel and scrolling down to the 'Thermal Compensation' option, which has a drop-down menu beside it that is set to Enabled by default. Use the drop-down to change the setting to Disabled and then start the depth stream.
-
The room temperature is stable. I do not know how the temperature change because I did not touch the camera. Does the RealSense SDK has an API to monitor the camera temperature?
My algorithm only relies on the left and right infrared images and I think the thermal compensation might not help.
-
You can track the current internal temperature of the camera in the Stereo Module > Controls section of the RealSense Viewer by looking at the 'API Temperature' and 'Projector Temperature' readings.
You can also retrieve these temperature values in the API with C++ or Python code.
C++
https://github.com/IntelRealSense/librealsense/issues/6735
Please sign in to leave a comment.
Comments
3 comments