RealSense Support

D405 and D435i

Comments

2 comments

  • MartyG

    Hi Yixun Liu  The D405 is designed for high image quality and high accuracy at close range (7 cm to 50 cm ideal depth range).  It can provide better results than the D435i at 10 cm (a distance where the depth image may have missing detail on the D435i model).

     

    Although the D405 is not equipped with a projector, you can compensate by either using a richly textured object or using an external visible projector (instead of an IR-based projector) to cast a texture onto the object's surface.  Visible projectors are discussed in the section of Intel's white-paper guide about using projectors with 400 Series cameras at the link below.

    https://dev.intelrealsense.com/docs/projectors#6-the-consumer-front-projector

     

     

     

    0
    Comment actions Permalink
  • Yixun Liu

    Very helpful.

    Thanks a lot!

    0
    Comment actions Permalink

Please sign in to leave a comment.