RealSense Support

D435 Custom RGB Sensor

Comments

1 comment

  • MartyG

    Hi Alal  you can find information about the interface that the sensors use by performing a word find operation in the 400 Series' data sheet document (at the link below) for the term mipi csi-2 

     

    https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet

     

    There was a past case about a custom build where a RealSense user speculated that other modules might work because "from my understanding these are just standard MIPI CSI-2 camera modules (OV9821 and OV2740), so any modules with similar spec (MP/s, etc.) should work".

     

    My understanding is that once the default sensor is replaced with a compatible module of your own choice then a Dynamic Calibration of the depth and RGB sensors should be performed.

     

    https://www.intel.com/content/www/us/en/download/645988/intel-realsense-d400-series-dynamic-calibration-tool.html

     

    Below is an example of the MIPI CSI-2 references in the data sheet.

     

     

    The RGB sensor used in the D435 camera model is OmniVision OV2740

     

     

    There is not information available regarding your question about resolution limits of a custom RGB sensor. RealSense supports a maximum RGB resolution of 1920x1080 

     

    An alternative to replacing the RGB module is to sync the RealSense camera's depth stream to an external non-RealSense high resolution RGB camera, making the RGB camera the 'master' and the RealSense depth camera the 'slave' in the multi-camera arrangement.

    0
    Comment actions Permalink

Please sign in to leave a comment.