RealSense Support

[D455] Difference Between Cameras

Comments

4 comments

  • MartyG

    Hi Nguyenduyduc14  Please try using the instructions in the link below to reset the camera calibration to factory-new defaults in the RealSense Viewer.  This is a different procedure to a hardware reset.

    https://github.com/IntelRealSense/librealsense/issues/10182#issuecomment-1019854487

    0
    Comment actions Permalink
  • Nguyenduyduc14

    Thanks, I got it.

    I have one more question.

    In IntelRealSenseViewer, we can restore factory but it only changes parameters of calibration.

    I see we have hardware reset will reset some setup like laser power, ... setup by number but they don't reset some setup kind of On, Off.

    Sometimes, I don't remember what is the default of these setups.

    Do we have a way the reset to default all setup in IntelRealSenseViewer?

    0
    Comment actions Permalink
  • MartyG

    The camera configuration json file 'DefaultPreset_D455.json' at the link below provides a list of D455 default values for a large range of settings, including the '156' default of the Laser Power setting.

    https://raw.githubusercontent.com/wiki/IntelRealSense/librealsense/d400_presets/DefaultPreset_D455.json

     

    The RealSense Viewer has an option to reset the Viewer program to its defaults (but not the camera, as that is reset by the Hardware Reset option).  You can find this by opening the Viewer's Settings panel by clicking on the gear wheel in the top corner of the window and selecting 'Settings' from its drop-down menu, then going to the General tab and clicking the Restore Defaults button.

     

     

    0
    Comment actions Permalink
  • Nguyenduyduc14

    Ok. I got it.

    Thanks

    0
    Comment actions Permalink

Please sign in to leave a comment.