View my account

d435i - save 3D model

Comments

9 comments

  • MartyG

    Hi Barakelisha098  Are you able to click on the Export option or is it grey and unresponsive?  The depth stream needs to be enabled in order for the Export option to be able to be clicked on.

     

    If the Export button does respond when clicked on, does an options box like the one in the image below appear?  And if the options box does appear, does clicking on 'Export' open a file selector window to choose a location to save the ply file to?

     

     

    0
    Comment actions Permalink
  • Barakelisha098

    "And if the options box does appear, does clicking on 'Export' open a file selector window to choose a location to save the ply file to?"

    This doesnt happen.

    0
    Comment actions Permalink
  • MartyG

    Thank you.  Have you tested the camera when directly accessing the Pi instead of using a VNC connection to see whether it may be the VNC connection that is causing the Export button to not function, please?

    0
    Comment actions Permalink
  • Barakelisha098

    When the camera connect to the computer the export button work, but in VNC  it is not..
    I saw the picture and the others button work..

    0
    Comment actions Permalink
  • MartyG

    I extensively researched the issue of the pop-up Export options not appearing but was not able to find a solution, unfortunately.

     

    If you left-click on the gear wheel icon in the top corner of the Viewer and select Settings from its drop-down menu, does the Settings panel pop up?  If it does not then this could suggest that there is a blocking issue with options in the Viewer that produce a pop-up overlay over the Viewer window when using VNC.

     

    0
    Comment actions Permalink
  • Barakelisha098

    I click on the gear wheel icon and I get a menu with 4 option..

    0
    Comment actions Permalink
  • MartyG

    The menu with 4 options dropping down when the gear wheel is clicked on is the correct behaviour.  Does the Settings panel in the image above appear if you click on the Settings menu option?

    0
    Comment actions Permalink
  • Barakelisha098

    Yes, it is appear when I click

    0
    Comment actions Permalink
  • MartyG

    Thanks very much.  It does appear that the problem that you are experiencing on a VNC Viewer connection is specifically affecting the ply Export option and not the other options.  There is not an available solution for this except for writing your own point cloud generation and ply export script instead of exporting a ply from the Viewer.

     

    You could also test whether installing a different VNC tool on your Pi than the VNC Viewer resolves the issue with the Export button.

    0
    Comment actions Permalink

Please sign in to leave a comment.