RealSense Support

D401 module questions

Comments

1 comment

  • MartyX Grover

    1.  The EEPROM flash memory storage chip that the calibration data is written to is on the camera depth module board.  This is confirmed in a table at the top of page 45 of the current edition of the 400 Series data sheet document.

    https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet

    Once the depth module and the Vision Processor D4 Board have been joined together with the interposer, perform a calibration and write it to the camera hardware.

     

    2.  The D401 must be paired with the V4 version of the Vision Processor D4 Board because of the D401's ability to stream RGB from the depth sensor instead of having a separate RGB sensor and enhance it with the Image Signal Processor (ISP).  It therefore cannot be used with other Vision Processor D4 Board versions.

     

    3.  The rigid interposer board product performs the same function as a flexible interposer cable such as the HSF cable products, yes.  The cables provide the advantage of being able to orient the camera and D4 boards to fit a certain space within a housing such as a product casing or a robot frame.

     

    4.  Page 50 of the data sheet lists the RealSense camera models that are compatible with the flexi and rigid interposers, which does not include the D401 model.  Pages 54-57 list the design details of the D401 interposer if you are able to construct your own cable, and contact details at the bottom of page 57 for ordering a custom-made interposer flexi cable from a company called Cocom Consumer Electronics Ltd.

    0
    Comment actions Permalink

Please sign in to leave a comment.