RealSense Support

Box dimensioner issue

Comments

4 comments

  • MartyX Grover

    Hi Javi0798  I would speculate that you could create a function that is called when a button-click event occurs, and save the color image with the OpenCV imwrite instruction.  Assuming that you will be using Python if you are adapting the box_dimensioner_multicam.py example, the link below has an example of Python code for saving the color image with imwrite.

    https://support.intelrealsense.com/hc/en-us/community/posts/360052346893-RGB-image-captured-by-Intel-realsense-camera-is-dark-using-python-code-

    0
    Comment actions Permalink
  • Javi0798

    I have tried, but what I receive is a simple screenshot of the chessboard and not of the measures of the box that is what I want. Here is the code.

    # Import RealSense, OpenCV and NumPy
    import pyrealsense2 as rs
    import cv2
    import numpy as np
    from PySide2.QtWidgets import QApplication, QMainWindow, QComboBox, QWidget, QDialog
    from PySide2.QtUiTools import QUiLoader
    from PySide2.QtCore import QAbstractAnimation, QFile
    from lxml import etree as et
     
    # Import helper functions and classes written to wrap the RealSense, OpenCV and Kabsch Calibration usage
    from collections import defaultdict
    from realsense_device_manager import DeviceManager
    from calibration_kabsch import PoseEstimation
    from helper_functions import get_boundary_corners_2D
    from measurement_task import calculate_boundingbox_points, calculate_cumulative_pointcloud, visualise_measurements
    import sys
    from ui_configuracion import Ui_Dialog_Config
    from ui_capturar import Ui_Dialog_Capturar
    from ui_guardar import Ui_Dialog_Guardar
     
    class Configuracion(QDialog):
    	def __init__(self):
    		super(Configuracion, self).__init__()
    		self.ui=Ui_Dialog_Config() 
    		self.ui.setupUi(self)
    		self.ui.lineEdit.setText("7")
    		self.ui.lineEdit_2.setText("7")
    		self.ui.lineEdit_3.setText("0.0353")
    		self.ui.pushButton.clicked.connect(self.ejecutar_demo)
    		self.ui.pushButton.clicked.connect(self.quit_app)
    		
    	
    	def quit_app(self):
    		self.hide()	
    		
    	def ejecutar_demo(self):
    		
    		self.chessboard_width=int(self.ui.lineEdit.text())
    		self.chessboard_height=int(self.ui.lineEdit_2.text())
    		self.square_size=float(self.ui.lineEdit_3.text())
    		self.quit_app()
    		self.run_demo(self.chessboard_width, self.chessboard_height, self.square_size)
     
    	def run_demo (self, ch_width, ch_height, sq_size):
    	
    		# Define some constants 
    		L515_resolution_width = 1024 # pixels
    		L515_resolution_height = 768 # pixels
    		L515_frame_rate = 30
     
    		resolution_width = 1280 # pixels
    		resolution_height = 720 # pixels
    		frame_rate = 15  # fps
    
    		dispose_frames_for_stablisation = 30  # frames
    
    		try:
    			# Enable the streams from all the intel realsense devices
    			L515_rs_config = rs.config()
    			L515_rs_config.enable_stream(rs.stream.depth, L515_resolution_width, L515_resolution_height, rs.format.z16, L515_frame_rate)
    			L515_rs_config.enable_stream(rs.stream.infrared, 0, L515_resolution_width, L515_resolution_height, rs.format.y8, L515_frame_rate)
    			L515_rs_config.enable_stream(rs.stream.color, resolution_width, resolution_height, rs.format.bgr8, frame_rate)
     
    			rs_config = rs.config()
    			rs_config.enable_stream(rs.stream.depth, resolution_width, resolution_height, rs.format.z16, frame_rate)
    			rs_config.enable_stream(rs.stream.infrared, 1, resolution_width, resolution_height, rs.format.y8, frame_rate)
    			rs_config.enable_stream(rs.stream.color, resolution_width, resolution_height, rs.format.bgr8, frame_rate)
     
    			# Use the device manager class to enable the devices and get the frames
    			device_manager = DeviceManager(rs.context(), rs_config, L515_rs_config)
    			device_manager.enable_all_devices()
    		
    			# Allow some frames for the auto-exposure controller to stablise
    			for frames in range(dispose_frames_for_stablisation):
    				frames = device_manager.poll_frames()
     
    			assert( len(device_manager._available_devices) > 0 )
    			"""
    			1: Calibration
    			Calibrate all the available devices to the world co-ordinates.
    			For this purpose, a chessboard printout for use with opencv based calibration process is needed.
    		
    			"""
    			# Get the intrinsics of the realsense device 
    			intrinsics_devices = device_manager.get_device_intrinsics(frames)
    		
    					# Set the chessboard parameters for calibration 
    			chessboard_params = [ch_height, ch_width, sq_size] 
    		
    			# Estimate the pose of the chessboard in the world coordinate using the Kabsch Method
    			calibrated_device_count = 0
    			while calibrated_device_count < len(device_manager._available_devices):
    				frames = device_manager.poll_frames()
    				pose_estimator = PoseEstimation(frames, intrinsics_devices, chessboard_params)
    				transformation_result_kabsch  = pose_estimator.perform_pose_estimation()
    				object_point = pose_estimator.get_chessboard_corners_in3d()
    				calibrated_device_count = 0
    				for device_info in device_manager._available_devices:
    					device = device_info[0]
    					if not transformation_result_kabsch[device][0]:
    						print("Place the chessboard on the plane where the object needs to be detected..")
    					else:
    						calibrated_device_count += 1
     
    			# Save the transformation object for all devices in an array to use for measurements
    			transformation_devices={}
    			chessboard_points_cumulative_3d = np.array([-1,-1,-1]).transpose()
    			for device_info in device_manager._available_devices:
    				device = device_info[0]
    				transformation_devices[device] = transformation_result_kabsch[device][1].inverse()
    				points3D = object_point[device][2][:,object_point[device][3]]
    				points3D = transformation_devices[device].apply_transformation(points3D)
    				chessboard_points_cumulative_3d = np.column_stack( (chessboard_points_cumulative_3d,points3D) )
     
    			# Extract the bounds between which the object's dimensions are needed
    			# It is necessary for this demo that the object's length and breath is smaller than that of the chessboard
    			chessboard_points_cumulative_3d = np.delete(chessboard_points_cumulative_3d, 0, 1)
    			roi_2D = get_boundary_corners_2D(chessboard_points_cumulative_3d)
     
    			print("Calibration completed... \nPlace the box in the field of view of the devices...")
     
     
    			"""
    					2: Measurement and display
    					Measure the dimension of the object using depth maps from multiple RealSense devices
    					The information from Phase 1 will be used here
     
    					"""
     
    			# Enable the emitter of the devices
    			device_manager.enable_emitter(True)
     
    			# Load the JSON settings file in order to enable High Accuracy preset for the realsense
    			device_manager.load_settings_json("/HighResHighAccuracyPreset.json")
     
    			# Get the extrinsics of the device to be used later
    			extrinsics_devices = device_manager.get_depth_to_color_extrinsics(frames)
     
    			# Get the calibration info as a dictionary to help with display of the measurements onto the color image instead of infra red image
    			calibration_info_devices = defaultdict(list)
    			for calibration_info in (transformation_devices, intrinsics_devices, extrinsics_devices):
    				for key, value in calibration_info.items():
    					calibration_info_devices[key].append(value)
     
    			# Continue acquisition until terminated with Ctrl+C by the user
    			pipeline = rs.pipeline()
    			config = rs.config()
    			config.enable_stream(rs.stream.color, 1280, 720, rs.format.bgr8, 30)
    			profile = pipeline.start(config)
    			#self.frames_devices = device_manager.poll_frames()
    			self.frames = pipeline.wait_for_frames()
    			align_to = rs.stream.color
    			align = rs.align(align_to)
    			aligned_frames = align.process(self.frames)
    			color_frame = aligned_frames.get_color_frame()
    			self.color_image = np.asanyarray(color_frame.get_data())
    			dialog_capturar=capturar()
    			dialog_capturar.ui.pushButton.clicked.connect(self.f1)
    			dialog_capturar.ui.pushButton.clicked.connect(self.quit_app)
    			dialog_capturar.show()
    			while 1:
    				 # Get the frames from all the devices
    					frames_devices = device_manager.poll_frames()
     
    					# Calculate the pointcloud using the depth frames from all the devices
    					point_cloud = calculate_cumulative_pointcloud(frames_devices, calibration_info_devices, roi_2D)
     
    					# Get the bounding box for the pointcloud in image coordinates of the color imager
    					bounding_box_points_color_image, self.length, self.width, self.height = calculate_boundingbox_points(point_cloud, calibration_info_devices )
    					
    					# Draw the bounding box points on the color image and visualise the results
    					visualise_measurements(frames_devices, bounding_box_points_color_image, self.length, self.width, self.height)
     
    				
    		except KeyboardInterrupt:
    			print("The program was interupted by the user. Closing the program...")
    	
    		finally:
    			device_manager.disable_streams()
    			cv2.destroyAllWindows()
     
    	def f1(self):
    		
    		dialog_guardar = guardar(self.length, self.width, self.height, self.color_image)
    		dialog_guardar.exec()
     
     
    class capturar(QDialog):
    	def __init__(self):
    		super(capturar, self).__init__()
    		self.ui=Ui_Dialog_Capturar()
    		self.ui.setupUi(self)
    		
     
    class guardar(QDialog):
    	def __init__(self, length, width, height, frames_devices):
    		super(guardar, self).__init__()
    		self.ui=Ui_Dialog_Guardar()
    		self.ui.setupUi(self)
    		longitud=int(length*10000)
    		anchura=int(width*1000)
    		altura=int(height*1000)
    		self.ui.lineEdit.setText(str(longitud))
    		self.ui.lineEdit_2.setText(str(anchura))
    		self.ui.lineEdit_3.setText(str(altura))
    		cv2.imwrite('C:/carpetas/out.jpg', frames_devices) 
    
    0
    Comment actions Permalink
  • MartyX Grover

    I thought that there was a possibility that this might occur, since the overlaid coordinate writing is applied to the color image within a loop at the part of the box_dimensioner_multicam script linked to below.

    https://github.com/IntelRealSense/librealsense/blob/master/wrappers/python/examples/box_dimensioner_multicam/box_dimensioner_multicam_demo.py#L144

    This implies that the imwrite instruction might need to be placed directly after this line.  The problem is setting up a mechanism so that it only triggers when a button input is made.

    Perhaps it could be tested by putting the imwrite code inside the keyboard interrupt code block.

    https://github.com/IntelRealSense/librealsense/blob/master/wrappers/python/examples/box_dimensioner_multicam/box_dimensioner_multicam_demo.py#L147

     

    On the other hand, the text overlay gives me the impression that it is overlaying the text on top of the window displaying the color image rather than incorporating it into the image data itself, hence why it is not included in an exported image file.

    0
    Comment actions Permalink
  • MartyX Grover

    Rather than saving the image from the camera, an alternate approach may be to use general Python code to capture the contents of a specific window (and not capture the entire screen).  The link below is a tutorial that uses a Python module called pygetwindow to do so.

    https://www.thepythoncode.com/article/record-a-specific-window-in-python

    0
    Comment actions Permalink

Please sign in to leave a comment.