RealSense Support

D435i misrecognizes louver as short range

Comments

1 comment

  • MartyX Grover

    Hi Syuuji Harada

    The D435i is possibly interpreting the slats of the air conditioner grille as a repetitive pattern (an observed area of the scene with similar looking parts that repeat horizontally and vertically, such as a horizontal row of fence posts or a vertical stack of window blind slats).  Repetitive patterns can confuse the depth sensing of the camera.

     

    The link below suggests information resources for reducing the negative effects of repetitive patterns.

    https://github.com/IntelRealSense/librealsense/issues/6713#issuecomment-651114720

    Putting the camera at a higher height and tilting it downwards at an angle towards the air conditioner instead of facing directly ahead may also help to break up the recognized pattern.  A tilt should not negatively impact the depth measurement as long as the tilt angle is not greater than 30 degrees.

    0
    Comment actions Permalink

Please sign in to leave a comment.