RealSense Support

Questions about D415 accuracy

Comments

1 comment

  • MartyX Grover

    Hi Dzhus  Thanks very much for your questions.

    1. Depth measurement error starts at around zero at the camera and increases linearly over distance.  This phenomenon is called RMS Error.  On the D435 / D435i camera models, error increases at a rate that is approximately 2x that of D415, meaning that at around 1.5 meters D415 and D435 / D435i will have similar levels of error, with D415 having a little less.  The greater the distance from the camera, the greater the difference in error will become.

    Section 5.  Understand theoretical limit of Intel's camera tuning guide linked to below provides further information about RMS Error and a graphical chart demonstrating the D415 and D435 /D435i error change over distance.

    https://dev.intelrealsense.com/docs/tuning-depth-cameras-for-best-performance#section-verify-performance-regularly-on-a-flat-wall-or-target

     

    2.  Whilst RMS Error is one of the factors that can generate error, there are also other environmental and lighting factors that can contribute to error too. 

    Examples are fluorescent lights such as ceiling strip lights, and aspects in the observed scene that represent a 'repetitive pattern' of repeating horizontal or vertical elements, such as a horizontal row of fence posts or a vertical stack of window blind stats. There are usually methods that can be employed to reduce particular types of error though.

     

    3.  A 2x2 cm cube may be difficult to isolate from the rest of the scene around it at 1.5 meters range.  It may help if the cube has a textured surface instead of being plain and smooth, as a textured surface will be more easily analysable for depth information.

    0
    Comment actions Permalink

Please sign in to leave a comment.