RealSense Support

D405 Focus and Depth of Field vs D430?

Comments

2 comments

  • MartyX Grover

    Hi Henry, my understanding is that the smaller baseline of the D405 is part of what allows the image to remain in focus down to 7 cm without blurring.  The larger baseline of the D430 could cause the image to blur at the same distance, even if you used a disparity shift to reduce the D430's minimum depth sensing distance from its default 0.1 meters / 10 cm down to 7 cm.

     

    The D430 does not have an RGB sensor though and also does not support streaming of color from its infrared sensor.    Can you confirm that you have a D430 please and not a D435 (which does have an RGB sensor).

     

    If you had a RealSense camera with an RGB sensor such as D435 then you could sharpen a blurry RGB image by maximizing the value of the RealSense SDK's Sharpness RGB option to '100', as demonstrated in the link below with the barcode on a drink bottle.

    https://github.com/IntelRealSense/librealsense/issues/7187#issuecomment-690248295

     

    I tested the D405 with another drink bottle at various distances without altering the default Sharpness value  of '50'.  At the minimum 7 cm distance from the barcode the RGB image clarity is excellent.

     

     

    I then moved the camera furter away and captured at 15 cm intervals up unti 45 cm.  This should provide an indication of how a checkerboard image may be rendered at various distances at default Sharpness.

     

    At 15 cm:

     

     

    At 30 cm:

     

     

    At 45 cm:

     

    0
    Comment actions Permalink
  • Henry

    Thanks yes I do have a D435 - sorry for the error.  Increasing sharpness does seem to help so I will use that but the D405 seems to focus a lot closer so may be a better solution though without a dot projector we will need to test.

    0
    Comment actions Permalink

Please sign in to leave a comment.