RealSense Support

The d455 camera cannot recognize objects beyond a distance of approximately 2.5 meters, and the background image will turn completely black

Comments

2 comments

  • MartyX Grover

    Hi L cong  In the RealSense Viewer tool, a post-processing filter called the 'Threshold Filter' is enabled by default.  It adjusts the depth data to exclude all data with a distance greater than 4 meters.

     

    You can disable the filter so that the camera can see to its full depth range (up to 20 meters on the D455 model) by going to the Stereo Module > Post-Processing Filters section of the Viewer's options side-panel and left-clicking on the blue icon beside 'Threshold Filter' in the list of filters to turn the filter off so it can display depth beyond 4 meters.

    1
    Comment actions Permalink
  • L cong

    Okay, I'll have a try, Thank you very much.

    0
    Comment actions Permalink

Please sign in to leave a comment.