d455 firmware change bricked the camera
Hello! I have thos exact issue as documented in the following post:
I followed all the troubleshooting as descrived in this post and camera is still not working.
In summary the D455 camera became undetectable after a firmware update and could not be found by the Windows Device Manager or a range of different RealSense applications, such as the RealSense Viewer, Dynamic Calibrator and rs-fw-update. The RGB stream could not be accessed outside of the SDK in the Camera app of Windows. The Windows hardware troubleshoot tool was also unable to resolve the problem.
The two RealSense drivers (RGB and Depth) do not appear under the Cameras category of the Device Manager, and the Manager shows the camera as 'Unknown USB Device (invalid Configuration Descriptor)'.
Help!
-
Hi Vjbirds You mentioned in the case that you linked to that you tried to use rs-fw-update in its Recovery mode (-r) to restore the camera. The command used in that case was rs-fw-update -r -f Signed_Image_UVC_5_12_12_100.bin
Did you use this firmware version 5.12.12.100 or a different firmware .bin file when using the command, please? If a different firmware, which one did you use?
-
It does appear that this camera may be a "bricked" device, in which case it may be best dealt with via a private support ticket as you suggested in your original message on the other case that you posted on. Though I am an Intel RealSense Support Engineer, I am not a member of this Intel RealSense Customer Support forum's staff (I am on a different RealSense support team) and so cannot myself handle issues on this forum that potentially involve a camera return / replace.
I would therefore recommend creating another new case on this forum to explain that the camera is not detectable and that you would like to request a support ticket with an Intel RealSense Customer Support forum team member, posting links to the previous case and this one to illustrate that the issue has been carefully explored already and not yet resolved. Your issue should then get picked up by a team member of this forum.
Please sign in to leave a comment.


Comments
9 comments