RealSense Support

Intel realsense d435i camera

Comments

1 comment

  • MartyX Grover

    Hi Themis Gate7  RealSense 400 Series cameras are compatible with any computer / computing device with an Intel or Arm processor.

    The Up Board range has a long history of compatibility with RealSense cameras dating back to 2015.  The original Up Board could be used with an R200 stereo depth camera (the original predecessor of the 400 Series stereo depth cameras, such as the D435i).  Stronger specifications can have more cameras active simultaneously.  For example, an Up Squared model can handle two 400 Series cameras.

    0
    Comment actions Permalink

Please sign in to leave a comment.