Intel realsense d435i camera
Hey everyone,
I currently own the d435i depth camera and I was thinking to buy the "Up Xtreme" board with the Intel CPU. Does anyone knows if the camera is compatible with the board and if I'll have a problem with the installation?
Thanks in advance.
-
Hi Themis Gate7 RealSense 400 Series cameras are compatible with any computer / computing device with an Intel or Arm processor.
The Up Board range has a long history of compatibility with RealSense cameras dating back to 2015. The original Up Board could be used with an R200 stereo depth camera (the original predecessor of the 400 Series stereo depth cameras, such as the D435i). Stronger specifications can have more cameras active simultaneously. For example, an Up Squared model can handle two 400 Series cameras.
Please sign in to leave a comment.
Comments
1 comment