RealSense Support

Using realsense-ros wrapper with D555 over Ethernet

Comments

10 comments

  • MartyX Grover

    Hi Niklas Schlueter  Launching the ROS2 wrapper in D555's DDS ethernet mode is supported.  If your camera has firmware driver.  I note though that you are using librealsense and wrapper versions that are newer than the current latest master releases, which at the time of writing this are librealsense 2.57.7 and wrapper 4.57.6.  Did you build your .58.1 versions using the /r branches below, please?

    https://github.com/realsenseai/librealsense/tree/r/2.58.1

    https://github.com/realsenseai/realsense-ros/tree/r/4.58.1

     

    I would first recommend testing whether ROS topics are accessible at all on your D555 by using ros2 topic list without launching the rs_launch.py wrapper.  The camera should be able to publish a small list of DDS topics without the wrapper being active that resembles the list below.

     

    /parameter_events
    /realsense/D555_342622302478_Color
    /realsense/D555_342622302478_Depth
    /realsense/D555_342622302478_Infrared_1
    /realsense/D555_342622302478_Infrared_2
    /realsense/D555_342622302478_Motion
    /rosout

     

     

    0
    Comment actions Permalink
  • Niklas Schlueter

    Hello,
    Thanks for the quick reply. Actually, after restarting my computer and camera it magically started working. The wrapper ran successfully and I can also see the standard DDS topics you have mentioned.
    Regarding your question: Yes, I used the r/ branches to build the sdk and wrapper myself as I though there might be an issue with the version that you can install via apt.

    To make sure the issue still exists I have also tried it on the version installed  through the tutorials (SDK) https://github.com/realsenseai/librealsense/blob/master/doc/distribution_linux.md#installing-the-packages and (wrapper) https://github.com/realsenseai/realsense-ros#option-1-install-debian-package-from-ros-servers-foxy-eol-distro-is-not-supported-by-this-option

    By running rs-enumerate-devices in a terminal where I have ros jazzy initialised I get

    $ /opt/ros/jazzy/bin/rs-enumerate-devices --version
    /opt/ros/jazzy/bin/rs-enumerate-devices  version: 2.57.7.0
    $ /opt/ros/jazzy/bin/rs-enumerate-devices
    No device detected. Is it plugged in?

    But in a terminal that does not have ros initialised I can run the sdk's rs-enumerate-devices

    $ /bin/rs-enumerate-devices --version
    /bin/rs-enumerate-devices  version: 2.57.7.10378
    $ /bin/rs-enumerate-devices
    Device info:
     Name                          :     Intel RealSense D555
     Serial Number                 :     342622301250
     Firmware Version              :     7.56.37776.6014
     Physical Port                 :     realsense/D555_342622301250
     Product Id                    :     DDS
     Camera Locked                 :     YES
     Product Line                  :     D500
     Firmware Update Id            :     342622301250
     Connection Type               :     DDS
    Imu Type                      :     BMI088

    Stream Profiles supported by RGB Camera
    ...

    However, once I initialise the ros environment, the rs-enumerate-devices command seems to use one of the libraries installed in ros, which makes it not detect any devices. Could there be an issue with the libraries in ros?

    $ ldd /bin/rs-enumerate-devices | grep realsense
    librealsense2.so.2.57 => /lib/x86_64-linux-gnu/librealsense2.so.2.57 (0x0000778e37000000)
    $ source /opt/ros/jazzy/setup.sh
    $ ldd /bin/rs-enumerate-devices | grep realsense
    librealsense2.so.2.57 => /opt/ros/jazzy/lib/x86_64-linux-gnu/librealsense2.so.2.57 (0x0000760ee6a00000)
    $ /bin/rs-enumerate-devices
    No device detected. Is it plugged in?
    $ /bin/rs-enumerate-devices --version
    /bin/rs-enumerate-devices  version: 2.57.7.10378

    At the same time DDS topics are still transmitted and received:

    $ ros2 topic list
    parameter_events
    /realsense/D555_342622301250/tf_static
    /realsense/D555_342622301250_Color
    ...
    $ ros2 topic hz /realsense/D555_342622301250_Color
    average rate: 29.965
        min: 0.028s max: 0.038s std dev: 0.00170s window: 32
    average rate: 29.984
        min: 0.028s max: 0.038s std dev: 0.00121s window: 63

    And thus the wrapper of course cannot find the device aswell:

    $ ros2 launch realsense2_camera rs_launch.py
    [INFO] [launch]: All log files can be found below /home/user/.ros/log/2026-05-07-12-04-00-546235-user-ubuntu-tower-12820
    [INFO] [launch]: Default logging verbosity is set to INFO
    [INFO] [launch.user]: 🚀 Launching as Normal ROS Node
    [INFO] [realsense2_camera_node-1]: process started with pid [12832]
    [realsense2_camera_node-1] [INFO] [1778148240.923083879] [camera.camera]: RealSense ROS v4.57.7
    [realsense2_camera_node-1] [INFO] [1778148240.923157283] [camera.camera]: Built with LibRealSense v2.57.7
    [realsense2_camera_node-1] [INFO] [1778148240.923169340] [camera.camera]: Running with LibRealSense v2.57.7
    [realsense2_camera_node-1] [WARN] [1778148240.940575921] [camera.camera]: No RealSense devices were found!
    0
    Comment actions Permalink
  • MartyX Grover

    The recommended method of installing the librealsense SDK for use with DDS is to build it with source code with CMake using the 'installation.md' instructions and include the flag -DBUILD_WITH_DDS=ON in the CMake build instruction.

    https://github.com/realsenseai/librealsense/issues/14284#issuecomment-3349204762

     

    And then build the ROS wrapper from source code with colcon build using the Option 2 instructions instead of the Option 1 package installation instructions.

     

    However, you should be able to test whether DDS is working well on your computer just by installing librealsense with DDS enabled in the CMake build instruction.  This is because the 7.56.37776.6014 firmware driver that you have installed in your camera has support for native ROS. 

     

    This means that you can launch a data visualization application such as realsense-viewer and then change the image in the visualization application (e.g the Viewer) by inputting commands such as 'ros2 param set' ones into the ROS2 terminal without having to have the ROS2 wrapper installed and launched.

    0
    Comment actions Permalink
  • Niklas Schlueter

    So that means DDS is not supported with the ROS installation available via apt? As mentioned before, the SDK seems to work without any issues in both cases, installing it via apt or building manually with the DBUILD_WITH_DDS flag.
    It appears that the ROS wrapper version 4.58.1 is the issue. If installing via apt is not recommended, I can just work with the newer versions, which run perfectly fine. But of course it would be easier to use the apt installation for the setup in my organisation.

    Regarding your advice with the use of the native ROS support: Maybe I am missing something, but when you use the camera without the wrapper, there is no node running in my local ROS system. How should I then change something via ros2 param set? Of course the topics are transmitted via DDS, but I'm still missing a way to interact with the camera without having a wrapper or node in any other kind running in my local ROS.
    Of course the wrapper and realsense-viewer use some kind of interface to communicate with the camera. Is this available as a non GUI application, which can be used by scripts or similar, or is it required to use either the realsense-viewer or the wrapper to change preferences for the camera behaviour?

    0
    Comment actions Permalink
  • MartyX Grover

    To use librealsense applications such as realsense-viewer on a DDS connection, it should be necessary to build librealsense from source code with the -DBUILD_WITH_DDS=ON flag.  

     

    In regard to ROS2 though, the D555 camera has built-in 'plug and play' integration with ROS2, making a short list of DDS topics available for streaming to ROS2 nodes without requiring additional SDK or wrapper installation.

     

    As you are using the .6014 firmware with native ROS support, you can use ros2 param set without a node such as the wrapper by including the unique /D555 number in the DDS topics (which is based on the camera's serial number) in the param command.  For example, your topic list includes the one below: 

    /realsense/D555_342622301250_Color

     

    So you can use a ros2 param set command like the example below that disables auto-exposure:

    ros2 param set /D555_342622301250 RGB.option.Enable_Auto_Exposure 0

     

    You can obtain a list of available parameters to use with ros2 param set with the ros2 param list command.

     

    Parameters can also be changed with program scripting after the ROS2 wrapper has been launched, using a Python node script like the ones at the link below.  This requires wrapper installation though.

    https://github.com/realsenseai/realsense-ros/tree/ros2-master/realsense2_camera/scripts

    0
    Comment actions Permalink
  • Niklas Schlueter

    I have been building the SDK with the -DBUILD_WITH_DDS=ON flag. It seems that the SDK is working well, as rs-enumerate-devices reliably shows the camera. But the ros wrapper does not work still. In very few instances it is able to detect the camera, but it is not reproducible and in the vast majority of attempts it will not find the camera. I have no idea what the cause could be. If you have any information on how to get the wrapper to run with DDS, I'd be very thankful.

    Regarding your comment about setting the parameter: It does not work for me. I get the following output:

    ros2 param set /realsense/D555_342622301250 RGB.option.Enable_Auto_Exposure 0
    Node not found

    , which makes sense to me, as there is no node running without starting the wrapper.

    0
    Comment actions Permalink
  • MartyX Grover

    Does detection during ROS wrapper launch become any more reliable if you add initial_reset:=true to the launch command to reset the camera at launch?

     

    Is it detectable if you launch the wrapper node with ros2 run instead of ros2 launch?

    ros2 run realsense2_camera realsense2_camera_node --ros-args -p initial_reset:=true
    0
    Comment actions Permalink
  • MartyX Grover

    Hi Niklas Schlueter Do you require further assistance with this case, please?  Thanks!

    0
    Comment actions Permalink
  • Niklas Schlueter

    Hello,

    Please excuse the delay. I am only now getting back to this topic.
    I still have the same issue. In the meantime I have changed my manual installation to use the master branches of both the librealsense and realsense-ros repositories. I have followed the tutorials and your advice and built the SDK and wrapper manually. For the SDK I built with the DBUILD_WITH_DDS=ON flag.

    As said before, I can still see the camera via rs-enumerate-devices, but it is not detectable by the realsense2_camera node.
    It works in very few cases after unplugging and waiting for a little while before replugging. If the realsense2_camera node runs at the same time it can sometimes pick up the device. However, most of the times it still does not work and no device can be found.

    $ ros2 run realsense2_camera realsense2_camera_node --ros-args -p initial_reset:=true
    [INFO] [1783442505.660217498] [camera.camera]: RealSense ROS v4.58.2
    [INFO] [1783442505.660290972] [camera.camera]: Built with LibRealSense v2.58.2
    [INFO] [1783442505.660312413] [camera.camera]: Running with LibRealSense v2.58.2
    [WARN] [1783442508.695100225] [camera.camera]: No RealSense devices were found!
    [WARN] [1783442514.704580385] [camera.camera]: No RealSense devices were found!
    [WARN] [1783442520.713582994] [camera.camera]: No RealSense devices were found!
    ...

     

    $ rs-enumerate-devices 
    Device info: 
        Name                          :     Intel RealSense D555
        Serial Number                 :     342622301250
        Firmware Version              :     7.56.37776.6014
        Physical Port                 :     realsense/D555_342622301250
        Product Id                    :     DDS
        Camera Locked                 :     YES
        Product Line                  :     D500
        Firmware Update Id            :     342622301250
        Connection Type               :     DDS
        Imu Type                      :     BMI088

    Stream Profiles supported by RGB Camera
     Supported modes:
        STREAM           RESOLUTION     FORMAT      FPS
        Color            1280x800       RGB8        @ 30/15 Hz
        Color                |          RAW16       @ 15 Hz
     

    How can it be that it connects sometimes, but does not in most cases. I am not changing anything in the system or the setup. Additionally, if the node finds the camera, but then I restart the node, it again cannot find it.

    0
    Comment actions Permalink
  • MartyX Grover

    Discoverability of the D555 has been improving as new firmwares are released.  I would therefore recommend updating your 7.56.37776.6014 firmware to the current latest version 7.58.38448.10612 (which is also the recommended firmware for use with 2.58.2) to see if the rate of successful detections improves.

     

    I also recommend performing the firmware update  over a USB cable instead of ethernet if you have one.

    0
    Comment actions Permalink

Please sign in to leave a comment.