RealSense Support

Dynamic Calibrator

Comments

5 comments

  • MartyX Grover

    Hi Joe Haynes  The PDF user guide for the Dynamic Calibration tool states that firmware 5.10.6.0 and above is supported.  The guide has not been updated since 2021 though.  However, Dynamic Calibration version 2.6.4.0 was one of the first versions of the tool, released in 2018, so the 2021 guide's guidance about 5.10.6.0 and above being supported should in theory still be valid for that version of the tool.

     

    The 5.10.3.0 firmware was only one month older than 5.10.6.0 so that is likely why it is able to work with the tool.  It is not clear why it would accept 5.10.3.0 but have problems with the later 5.12.10.0.

     

    If you have access to a Windows computer then there is a more recent version of the tool you could try that can be downloaded from the link below.  The download of a zip file containing the Windows .exe installer program should start when the user agreement is accepted.

    https://dev.realsenseai.com/firmware-download/?file=42115

     

    RealSense has an alternative calibration toolset containing On-Chip and Tare calibration tools but these require a minimum of firmware 5.12.2.100 and so would not be usable with your firmwares.

     

    Another way to recalibrate a camera is to reset it to its factory-new calibration values.  Because of the age of your setup, you may have to do this using the Gold Reset mode of the CustomRW tool that is bundled with the Dynamic Calibration tool.  The CustomRW tool can be launched in gold reset mode on Ubuntu or Windows with the command below:

    Intel.Realsense.CustomRW -g

    0
    Comment actions Permalink
  • MartyX Grover

    Hi Joe Haynes Do you require further assistance with this case, please?  Thanks!

    0
    Comment actions Permalink
  • Joe Haynes

    Yes 

    I am still having problems running the Realsense Calibration tool, even the version you have mentioned above , as shown below 

     

    0
    Comment actions Permalink
  • MartyX Grover

    There was a past case of this start error reported in 2023.  A solution was not found in that case, unfortunately.  And the age of your firmware means that you will not be able to use the alternative On-Chip calibration tool that is built into the RealSense Viewer.

    https://support.realsenseai.com/hc/en-us/community/posts/13025891795987

     

    It is usually not necessary to perform a manual calibration of a new RealSense camera though as they are calibrated in the factory and so are already well calibrated when taken out of the box for first-time use.

    0
    Comment actions Permalink
  • MartyX Grover

    Do you have an update about this case that you can provide, please?  Thanks!

    0
    Comment actions Permalink

Please sign in to leave a comment.