RealSense Support

D455: The camera INFRARED-0 cannot be opened

Comments

4 comments

  • MartyX Grover

    Hello, are you attempting to open Infrared 0 - the left side infrared stream - as a UYVY RGB image whilst Infrared 1 - which is set to Y8 infrared - is open, please?  If you are then it will not be possible to access RGB color from Infrared 0.  This is because to access Infrared 0 color, Infrared 1 must be inactive.  Infrared 0 and 1 can only both be active simultaneously if both are set to an infrared format such as Y8 or Y16.

    0
    Comment actions Permalink
  • 财宾 杨
    Hello, thank you very much for your response! Now I want to achieve the goal of using two infrared cameras + IMU to collect data. Is this possible?
    The current problem is:
    1. The Format of INFRARED-0 has no options of Y8 and Y16, and it is impossible to open both IR-0 and IR-1 simultaneously.
    2. When opening IR-0 or IR-1 alone, only the left eye camera is activated.
    How should I solve this problem?

    0
    Comment actions Permalink
  • MartyX Grover

    If the USB connection is USB 2.1 then only Infrared 0 is supported.  A USB 3 connection is required for both Infrared 0 and Infrared 1 to be enabled simultaneously.

    0
    Comment actions Permalink
  • MartyX Grover

    Do you require further assistance with this case, please?  Thanks!

    0
    Comment actions Permalink

Please sign in to leave a comment.