View my account

Question about FoV geometry

Comments

4 comments

  • Marty Grover

    Hi Laurin Steiner  I would recommend not attempting to calculate your own FOV diagram or considering the invalid depth band due to the complexities involved.  It is much easier to work out the depth image's overall field of view by looking up its FOV value.  On the D456 it is 87 degrees wide (horizontal) and 58 degrees vertical (tall). 

     

    The depth image has its 0,0,0 origin at the centre-line of the left IR sensor, which is the sensor on the right-hand side of the camera when looking at it from the front.

     

     

    0
    Comment actions Permalink
  • Laurin Steiner

    Hello Marty Grover,

    Thank you for your response!
    I assume that the valid depth data in 3D space can then be measured using a geometry like this:

    As a conclusion, the valid depth-data field of view has the same geometry as each IR camera imager.

    Since this is a very important topic, I need confirmation regarding which depth-FoV geometry I can rely on. Based on your explanation, it would be the first option, correct?

    1. First option depth-FoV-geometry

    1. Second option depth-FoV-geometry



    Thank you very much.

    Best Regards

    Laurin

    0
    Comment actions Permalink
  • Marty Grover

    I located a reference which has an example of a diagram of the depth FOV triangle whose origin is the left-side IR sensor.

    https://github.com/realsenseai/librealsense/issues/2355#issuecomment-418712557

     

    The shape of the FOV shown in the diagram is for the D415 model rather than D456 but gives you a confirmation of the general triangular shape of a RealSense depth FOV viewpoint.  I would say that it most closely resembles your Option 1.

     

    The guide at the link below provides another example diagram of the RealSense depth FOV.

    https://docs.ros.org/en/iron/p/librealsense2/user_docs/depth-from-stereo.html

     

    0
    Comment actions Permalink
  • Laurin Steiner

    Thank you very much, that was really helpful!

    0
    Comment actions Permalink

Please sign in to leave a comment.