RealSense Support

D555 Not Working

Comments

3 comments

  • MartyX Grover

    Hi Marco Miralles  You mentioned that you have tried factory reset.  Have you tried the type of factory reset that is provided by the rs-dds-config tool while on a USB connection, please?

    https://github.com/realsenseai/librealsense/tree/master/tools/dds/dds-config

    rs-dds-config --factory-reset

     

    0
    Comment actions Permalink
  • Marco Miralles

    Hi Marty, thanks for the reply.

    I believe I had already tried factory resetting via the rs-dds-config utility and via the RealSense Viewer.

    I just tried factory resetting using the rs-dds-config as you mentioned and it is still not connecting via ethernet.

    I also heard from support and they said to RMA the camera through the store.

    C:\Users\CeCert\Downloads>rs-dds-config --factory-reset
    -I- [USB] Intel RealSense D555 s/n 419222301046, FW version 7.56.19919.4144
    -I-     MAC address: 0:0:0:0:0:0
    -I-     configured: 192.168.11.54 & 255.255.255.0 / 192.168.11.1 --> 192.168.11.55 & 255.255.255.0 / 192.168.11.1
    -I-     DDS:
    -I-         domain ID: 0
    -I-     link: OFF
    -I-         MTU, bytes: 9000
    -I-         timeout, ms: 4000
    -I-         priority: eth-first --> dynamic-eth-first
    -I-     DHCP: OFF
    -I-         timeout, sec: 30
    -I- Successfully changed
    -I- Resetting device...

    // Unplug and connect faulty camera via power/ethernet
    C:\Users\CeCert\Downloads>ping 192.168.11.55

    Pinging 192.168.11.55 with 32 bytes of data:
    Reply from 192.168.11.10: Destination host unreachable.
    Reply from 192.168.11.10: Destination host unreachable.
    Reply from 192.168.11.10: Destination host unreachable.
    Reply from 192.168.11.10: Destination host unreachable.

    Ping statistics for 192.168.11.55:
        Packets: Sent = 4, Received = 4, Lost = 0 (0% loss),

    // Reconnect working camera via power/ethernet
    C:\Users\CeCert\Downloads>ping 192.168.11.54

    Pinging 192.168.11.54 with 32 bytes of data:
    Reply from 192.168.11.54: bytes=32 time=902ms TTL=64
    Reply from 192.168.11.54: bytes=32 time<1ms TTL=64
    Reply from 192.168.11.54: bytes=32 time<1ms TTL=64
    Reply from 192.168.11.54: bytes=32 time<1ms TTL=64

    Ping statistics for 192.168.11.54:
        Packets: Sent = 4, Received = 4, Lost = 0 (0% loss),
    Approximate round trip times in milli-seconds:
        Minimum = 0ms, Maximum = 902ms, Average = 225ms


    C:\Users\CeCert\Downloads>rs-dds-config
    -I- [DDS] Intel RealSense D555 s/n 409122300551, FW version 7.56.19919.4144
    -I-     MAC address: 98:4f:ee:1b:13:32
    -I-     configured: 192.168.11.54 & 255.255.255.0 / 192.168.11.1
    -I-     DDS:
    -I-         domain ID: 0
    -I-     link: 1000 Mbps
    -I-         MTU, bytes: 9000
    -I-         timeout, ms: 4000
    -I-         priority: eth-first
    -I-     DHCP: OFF
    -I-         timeout, sec: 30

    0
    Comment actions Permalink
  • MartyX Grover

    Thanks very much for the update.  If a member of Support advised you to RMA return the camera to the store that you purchased it from then please proceed with that.

    0
    Comment actions Permalink

Please sign in to leave a comment.