View my account

Mobile Depth-Sensing

Comments

1 comment

  • MartyX Grover

    Hi Mercio Jonova  Thanks very much for your questions.

     

    1.  RealSense 400 Series cameras equipped with fast Global shutters on their sensors, such as D455, can handle depth sensing of movement as fast as a car travelling at full speed.  This is demonstrated in a YouTube video where a D435 is mounted to a moving car.

    https://www.youtube.com/watch?v=OwJmCyAn3JQ

     

    The IMU component is not involved in depth generation or stabilization.

     

    2.  The optimal depth sensing distance of D455 is up to 6 meters - in other words, depth accuracy is very good up until that distance before it starts noticeably drifting beyond that distance.

     

    3.  Noise / flickering may occur indoors if the camera is used in a location with overhead fluorescent type strip lighting.  Configuring a setting called Power Line Frequency can help to compensate for this interference.

     

    Outdoors, RealSense 400 Series cameras work very well in both bright-light and dim conditions.  If you have a scene where there are both bright and dim areas simultaneously, a feature called High-Dynamic Range (HDR) can be configured.

    https://dev.realsenseai.com/docs/high-dynamic-range-with-stereoscopic-depth-cameras

     

    If the camera is pointed directly at the sun then the sensors can become saturated with light, disrupting the images.  If you anticipate that the camera may regularly be pointed at the sun frequently, you could change to the D455f camera model that filters out sunlight or purchase the D455f's filter separately and fit it over the sensors on the outside of your current D455.

     

    4.  If you want to improve depth accuracy through calibration then the Tare tool should be used, as On-Chip improves depth quality.

    0
    Comment actions Permalink

Please sign in to leave a comment.