RealSense Support

Realsense viewer- Ability to preset settings

Comments

3 comments

  • MartyX Grover

    Hi Mderuijter  Not all settings that are defined in the RealSense Viewer are exported to a custom json, which may be why certain options such as Histogram Equalization do not update if you load the exported json file back into the RealSense Viewer, giving the impression that the import did not work when actually that particular option was not included in the json.

    In the link below, a RealSense team member explains to a RealSense user who also wanted to set Histogram Equalization with a json preset file that this option is not a hardware feature and is instead applied through the colorizer.

    https://github.com/IntelRealSense/librealsense/issues/1674#issuecomment-387361411

    Custom preset files cannot be stored in the camera hardware and are instead loaded into an application.  I researched your question carefully but cannot see a way to enable Histogram Equalization automatically in the Viewer on program start-up.  You could do so if you were writing your own application in a langauge such as C++ or Python.

    1
    Comment actions Permalink
  • Mderuijter

    Hi Marty, that was extremely helpful. Does this also apply to features such as the laser intensity, resolution, and frame rate.

    0
    Comment actions Permalink
  • MartyX Grover

    Although resolution and frame rate can be defined in a json with 'stream-height', 'stream-width' and 'stream-fps' parameters, in practice the camera pipeline will override the settings when streaming starts.  The usual approach to defining a custom resolution and FPS configuration for a program is to set the desired values as cfg (config) statements in the program's scripting.

     

    I do recall a case where a RealSense Python user demonstrated loading the cfg values for resolution and FPS into their custom stream configuration from a json though.

    https://support.intelrealsense.com/hc/en-us/community/posts/4406041385875-TKinter-python-with-librealsense2

     

    config.enable_stream(rs.stream.depth, int(jsonObj['stream-width']), int(jsonObj['stream-height']), rs.format.z16, int(jsonObj['stream-fps']))

    config.enable_stream(rs.stream.color, int(jsonObj['stream-width']), int(jsonObj['stream-height']), rs.format.bgr8, int(jsonObj['stream-fps']))

    cfg = pipeline.start(config)

     

    Another Python example of this method is at the link below:

    https://github.com/IntelRealSense/librealsense/issues/6075

     

    This method of loading json resolution and FPS values into the pipeline config to apply those values can likely be converted to C++ scripting, since the official C++ documentation for enable_stream in the link below describes the 'int' value system used in the Python code.

    https://intelrealsense.github.io/librealsense/doxygen/classrs2_1_1config.html#a7eac7c16b12a10f70ca93db62779ec1e

     

    Laser Power can be stored in a json exported from the Viewer via the 'controls-laserpower' parameter.  I confirmed with testing that when the exported json is applied in the Viewer, the Laser Power setting changes to the value stored in the json.

     

     

    0
    Comment actions Permalink

Please sign in to leave a comment.