d435i - transmit the data to computer
Hi ,
I have a d435i camera.
I want to transmit the data to my computer without a cable. How i can do that?
I will be glad if you can help me and thank you.
-
Hi Barakelisha098 Intel has a guide (in the link below) to setting up a RealSense camera as a Network Camera over ethernet cabling or wi-fi, with the camera attached to an affordable computing board such as Raspberry Pi 4 and the camera data sent to a central 'host' computer such as a laptop.
-
MartyG Thank you for the answer :)
I can use arduino instead Raspberry Pi ? -
The networking paper states that boards other than Pi can be used with the networking tool with minor modifications and cites Up Board as an example.
https://up-shop.org/up-board-series.html
I have not seen an example of an Arduino being used with the networking tool, though I would think that the most important factor is that the chosen board is able to run Linux as its OS, since the rs-server software component needs Linux in order to be compiled.
My research indicates that it is widely doubted that Arduino boards could run a Linux OS though because they are a microcontroller rather than a microprocessor.
Please sign in to leave a comment.
Comments
4 comments