RealSense Support

L515 - Can't get range over 2.5m

Comments

2 comments

  • Aznie Syaarriehaah

    Hi Jon Biggins,
    The Intel® RealSense™ LiDAR Camera L515 is designed to function best from 0.25 to 9 m at 95% reflectivity. The depth accuracy of the camera is as below:

    Depth error average at 1m distance from camera is <5mm*
    Depth error std deviation at 1m distance from camera is 2.5mm*
    Depth error average at 9m distance from camera is <14mm*
    Depth error st deviation at 9m distance from camera is 15.5mm*

    Meanwhile, could you share the screenshot of the viewer with the issue that you faced?

    Regards,
    Aznie
    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • 2410105798

    Hi, I have the same problem.
    My L515 was still working yesterday but suddenly I can't detect objects four meters away. I didn't change any settings, and the sensors didn't suffer any damage.  I rebooted the firmware but nothing improved.Would you please tell me how did you solve this problem?

    0
    Comment actions Permalink

Please sign in to leave a comment.