RealSense Support

Irregular errors in infrared stream of d435i during operation

Comments

3 comments

  • MartyX Grover

    Hi Johannes Abicht  The effect in your kindly provided infrared image is similar to one that was produced in the case linked to below, where the effect also occured periodically rather than all the time and was corrected with a reset or unplugging-replugging the USB cable.

    https://github.com/IntelRealSense/librealsense/issues/8880

     

    The RealSense user in that case found that the problem did not occur over a long-term period if the official 1 meter USB cable supplied with the camera was used.  Are you using the official cable or your own lengthier choice of cable, please?

    0
    Comment actions Permalink
  • Johannes Abicht

    Hi Marty,

    thanks for your fast reply and helpful link to the discussion - i keep that back in mind.

    In fact, we are using longer (5m) usb cables because the camera is mounted on top of the robot flange/gripper. 

    Are there further investigations corresponding to the cables, please?

    Johannes.

    0
    Comment actions Permalink
  • MartyX Grover

    When using longer cables with RealSense cameras, cable quality is important due to the volume of data that RealSense cameras transmit.  Ideally, premium quality 'industrial grade' cables that are proven for compatibility and stability with RealSense cameras should be used, such as the Newnex brand that the RealSense user in the linked case was using.

    https://www.newnex.com/realsense-3d-camera-connectivity.php

     

    If the cable is being moved around by the robot flange as it moves, a USB cable with a screw lock on its connector can be used to firmly fix the cable in the camera's USB port using the two small holes either side of the port on the side of the camera.

    0
    Comment actions Permalink

Please sign in to leave a comment.