(ZR300) Cant get the camera to load and run on linux 16.04 computer
Been trying all i could and nothing is happening. I cant load the intel realsense crossplatform api application
there is no terminal command list to run off of and its been a challenge.
I have a project due and i cant get the system to do what its meant to do.
please anyone help with what you can. I already tried github installation guides multiple of them. and sdk 2.0 didnt work. I have a (ZR300) older camera ---------- not SR300 newer camera
-
Hi Toa3dprinting The RealSense SDK 2.0 (also known as librealsense2) does not support the old ZR300 stereo depth camera model. SDK 2.0's predecessor SDK 'librealsense', which is now known as Legacy Librealsense, does support ZR300.
https://github.com/IntelRealSense/librealsense/tree/v1.12.1
There was also an SDK made only for ZR300 called RealSense SDK for Linux that had librealsense as its foundation and built upon it by adding numerous additional features. It is my understanding though that this SDK is now difficult to get working.
Please sign in to leave a comment.
Comments
1 comment