RealSense Support

D435 depth issue on object's edge?

Comments

1 comment

  • MartyX Grover

    Hi Mawin9587  The D435 that you are using is the most appropriate camera model for sensing at a 20 cm distance, as D435 and D435i have a minimum depth sensing distance of 0.1 meters (10 cm) that enables them to be positioned close to objects / surface.  Other camera models such as D415, D455 and L515 have a larger minimum depth sensing distance.  D435 and D435i are therefore best suited for very close range depth measurement.

    Which resolution are you using for depth, please?  The optimal depth accuracy resolution for D435/i is 848x480

     

    The discussion in the link below is a good reference regarding smoothing out waviness in point clouds that increases as the distance of the observed object from the camera increases.

    https://github.com/IntelRealSense/librealsense/issues/1375

     

    The link below discusses problems with observing flat surfaces from an angle.

    https://github.com/IntelRealSense/librealsense/issues/6857

     

    If you have an excess of empty area with no depth information on a point cloud, you may also find that a lot of that missing detail is filled in if you set the camera's depth unit scale to a value of '0.0001' instead of its default of '0.001'. 

    This can be tested in the RealSense Viewer program's 3D point cloud mode by adjusting the Depth Units option under the Controls sub-section of the Stereo Module options.  You can input 0.0001 manually by left-clicking on the pencil icon beside the option.

     

    0
    Comment actions Permalink

Please sign in to leave a comment.