View my account

Is the 82635AWGDVKPRQ software capable of creating point clouds?

Comments

1 comment

  • MartyX Grover

    Hi Jorge Gomez  Product number 82635AWGDVKPRQ refers to the RealSense D435 camera hardware product.  This camera, which is part of the '400 Series' camera range, is able to create point clouds using applications developed in the RealSense SDK software (also known as librealsense), such as the RealSense Viewer tool that is included free with the RealSense SDK.

    Shown below is an image of a 3D point cloud generated in the RealSense Viewer with a D435i camera model.  You can also write your own applications to generate a point cloud with the D435.  A range of languages are supported for application development, such as C++, Python and C#.

     

     

    0
    Comment actions Permalink

Please sign in to leave a comment.