RealSense D457 power supply
I can't seem to find anywhere what is the poweersupply needed for the D457 camera with fakra connector. The only information is that it is powered through the cable via PoC but not what voltage. My deserializer delivers 12v through the cable and I don't want to damage the product.
Any information on if the camera will handle that power supply and work properly?
-
Hi Václav Vachuška The GMSL / Fakra connector is part of the Vision Processor D4 circuit board inside the camera. The chart below, taken from page 23 of the data sheet document for the D457 camera model, states that the minimum supply voltage for the Fakra connector is 10.8 volts and the nominal voltage is 12 V, with a maximum of 13.2 V supported.
https://dev.realsenseai.com/docs/intel-realsense-d400-series-product-family-datasheet

Please sign in to leave a comment.
Comments
1 comment