RealSense Support

D456 Invalid SKU after Firmware update

Comments

3 comments

  • MartyG

    Hi Tobias Bolze  The minimum firmware supported by the D456 camera model is 5.15.0.2.  If an older firmware than the minimum supported version is installed then it can result in the Invalid SKU error. 

     

    The only alternative to voiding the warranty through disassembly is to contact the retailer that it was purchased from to enquire about an RMA return, as it is not a problem that can be fixed by users with software, unfortunately.

     

     

     

    0
    Comment actions Permalink
  • Tobias Bolze

    Hello Marty,

    Thank you for the quick Reply we tried to install Frimware 5.16.01 suggested by the sdk tool (See image with our other realsense d435, where same software is suggested).

    I think there is still no way to change, but I´m courius why it not worked.

    0
    Comment actions Permalink
  • MartyG

    Yes, the Invalid SKU problem should not have occurred when updating your D456 to the current latest firmware 5.16.0.1.

     

    Is the camera detected if you try to retrieve its information on Ubuntu with the 'rs-enumerate-devices' tool with the command rs-enumerate-devices -s

     

     

    0
    Comment actions Permalink

Please sign in to leave a comment.