View my account

D455 with raspberry pi 4 and ros2

Comments

1 comment

  • MartyG

    Hi Pavan Vinay Chebrolu  The D455 camera model supports an alternative RGB mode called 'RGB from left infrared sensor' that can be used instead of the main RGB stream.  This can be used by setting the Infrared stream to RGB8 or BGR8 format instead of its default Y8 format and then enabling Infrared.

     

    Are you able to enable Depth and the Infrared stream's RGB mode, please?

    0
    Comment actions Permalink

Please sign in to leave a comment.