RealSense Support

Presence of leakage voltage in D435 series during hardware triggering

Comments

1 comment

  • Wai Fook Wan

    Hi Madhu Dhanasekaran,

    Thank you for reaching out to us.

     

    The issue appeared while providing a trigger pulse from a Raspberry Pi GPIO might be due to Raspberry Pi GPIO. Since there is no issue while you provided a trigger pulse from a push button with a 3.3/5V logic converter, the workaround would be using the push button with a 3.3V/5V logic converter.

     

    For more information on Using the Intel® RealSense™ Depth Cameras D400 Series in Multi-Camera Configurations, please refer to https://dev.intelrealsense.com/docs/multiple-depth-cameras-configuration.

     

     

    Regards,

    Wan

    Intel Customer Support

    0
    Comment actions Permalink

Please sign in to leave a comment.