RealSense Support

Performance evaluation with RealSense D435 in ROS2 humble (Intel® Robotics SDK)

Comments

3 comments

  • MartyG

    Hi Chic Lee  If you install the RealSense ROS2 wrapper at the link below then you can use the D435 with ROS2 Humble.

    https://github.com/IntelRealSense/realsense-ros

    0
    Comment actions Permalink
  • Chic Lee

    Hi MartyG,

    I know the RealSense ROS2 wapper and D435 works good with ROS2 Humble. 

    I want to know if D435 can hit specs with my RPL-S in ROS2 Humble.

    Can you provide more tips for this?

    0
    Comment actions Permalink
  • MartyG

    I would recommend first finding out the best performance that you can achieve with the default settings on your Raptor Lake S computer.  If performance is less than expected - for example, there is a drop in frames per second (FPS) speed or warning messages generating continuously in the terminal log - then you can then start trying various configuration settings to see whether performance and stability improves.

     

    For example, if you are experiencing lower than desired FPS then you could set a low resolution and FPS to determine whether higher resolution and FPS settings are reducing performance.

    ros2 launch realsense2_camera rs_launch.py depth_module.depth_profile:=640x480x15 rgb_camera.color_profile:=640x480x15 

     

    Another way to enhance performance is to build the ROS2 wrapper from source code with 'colcon build' and add the flag -DBUILD_ACCELERATE_GPU_WITH_GLSL to the colcon build command.  Doing so provides GPU acceleration of pointclouds and depth colorization.

    colcon build --cmake-args '-DBUILD_ACCELERATE_GPU_WITH_GLSL=ON'
    0
    Comment actions Permalink

Please sign in to leave a comment.