RealSense Support

D457 and GMSL FAKRA

Comments

4 comments

  • Munesh

    Hi Daniele,

    D457 Hardware Synchronization illustrates synchronization methods when multiple D457 cameras are being used on one system.

     

     

    Regards,

    Munesh

    0
    Comment actions Permalink
  • Daniele Lugli

    Hi Munesh, thank you for your reply.

     

    Anyway, as said in my original post, synchronization is not my concern at present. I am rather trying to figure out if and how several D457 (six in my case, in a range of max 12m from the hub) could be connected via GMSL/FAKRA, what would be the layout and the needed hardware, if a "normal" PC with Windows 11 could be used or if I need some nvidia box, how could be the power supply, and so on.

    The document you linked is interesting but it does not cover such questions - the example it presents considers only two D457.

    Thank you in advance for any further information and best regards.

    0
    Comment actions Permalink
  • Wai Fook Wan

    Dear Daniele Lugli,

    Since you need to connect six Intel® RealSense™ Depth Camera D457, you will need a platform that supports up to six GMSL camera interfaces. The following are a few platforms that support up to eight Intel® RealSense™ Depth Camera D457:

    For supported operating systems and power supply on the platforms above, please reach out to their technical support team.

     

    Best regards,

    Wan

    0
    Comment actions Permalink
  • Daniele Lugli

    Hi Wan,

    thank you for your prompt reply. I will examine the links you supplied, ask for prices too, and then give a feedback here.

    Best regards,

    Daniele

    0
    Comment actions Permalink

Please sign in to leave a comment.