L515 : from depth frame pixel to color frame pixel coordinate issue
#####################################################
## Read bag from file ##
#####################################################
# -*- coding: utf-8 -*-
# First import library
import pyrealsense2 as rs
# Import Numpy for easy array manipulation
import numpy as np
# Import OpenCV for easy image rendering
import cv2
# Import argparse for command-line options
import argparse
# Import os.path for file path manipulation
import os.path
import math
from scipy.ndimage import generic_filter
from time import sleep
from ultralytics import SAM
def draw_distance_with_arrows(image, p1, p2, text, color):
midpoint = ((p1[0] + p2[0]) // 2, (p1[1] + p2[1]) // 2)
cv2.arrowedLine(image, midpoint, ((p1[0] + midpoint[0]) // 2, (p1[1] + midpoint[1]) // 2), color, 2, tipLength=0.3)
cv2.putText(image, text, (midpoint[0] + 10, midpoint[1] - 10), cv2.FONT_HERSHEY_SIMPLEX, 0.6, color, 2)
def draw_angle(image, p1, p2, p3, angle, color,t):
# Draw lines from p2 to p1 and p2 to p3
#cv2.line(image, p2, p1, color, 1)
#cv2.line(image, p2, p3, color, 1)
# Draw the arc representing the angle inside
radius = 60 # Adjust the radius to fit inside
start_angle = np.degrees(np.arctan2(p1[1] - p2[1], p1[0] - p2[0]))
end_angle = np.degrees(np.arctan2(p3[1] - p2[1], p3[0] - p2[0]))
#Ensure the arc is drawn clockwise
if t==True :
#start_angle -= 360
start_angle = end_angle + 90
#start_angle = -1*start_angle +360
center = tuple(p2)
cv2.ellipse(image, center, (radius, radius), 0, end_angle, start_angle, color, 2)
# Display the angle value near the arc
angle_text = f"{angle:.1f}°"
text_position = (p2[0] - radius // 2, p2[1] - radius // 2)
cv2.putText(image, angle_text, text_position, cv2.FONT_HERSHEY_SIMPLEX, 0.6, color, 2)
# Function to calculate the angle between three points (p1, p2, p3)
def calculate_angle(p1, p2, p3):
v1 = np.array( [p1[0] - p2[0], p1[1] - p2[1], p1[2] - p2[2] ] )
v2 = np.array([p3[0] - p2[0], p3[1] - p2[1],p3[2] - p2[2]] )
angle_rad = np.arccos(np.dot(v1, v2) / (np.linalg.norm(v1) * np.linalg.norm(v2)))
angle_deg = np.degrees(angle_rad)
return angle_deg
def calculate_distance(p1, p2):
# Euclidean distance formula
return math.sqrt((p2[0] - p1[0]) ** 2 + (p2[1] - p1[1]) ** 2 + (p2[2] - p1[2]) ** 2 + (point2c[2] - point1c[2])**2)
# Initialize selected_points as an empty list to store selected points
selected_points = []
def reorder_rectangle_points(points):
# Convert points to a list of tuples and sort by Y-coordinate
points = sorted(points, key=lambda x: x[1]) # Sort by vertical position (Y)
# Separate into top and bottom points
top_points = sorted(points[:2], key=lambda x: x[0]) # Sort top points by X
bottom_points = sorted(points[2:], key=lambda x: x[0]) # Sort bottom points by X
# Return points in order: top-left, top-right, bottom-right, bottom-left
return np.array([top_points[0], top_points[1], bottom_points[1], bottom_points[0]])
def mouse_callback(event, x, y, flags, param):
global selected_points
# Scale back the coordinates to match the original registered frame
x_original = int(x )
y_original = int(y )
# Left click to add a point
if event == cv2.EVENT_LBUTTONDOWN:
if len(selected_points) == 2:
selected_points.pop(0) # Keep only the latest two points
selected_points.append((x_original, y_original))
# Right click to remove the last point
elif event == cv2.EVENT_RBUTTONDOWN and selected_points:
selected_points.pop()
# Create object for parsing command-line options
parser = argparse.ArgumentParser(description="Read recorded bag file and display depth stream in jet colormap.\
Remember to change the stream fps and format to match the recorded.")
# Add argument which takes path to a bag file as an input
parser.add_argument("-i", "--input", type=str, help="C:/Users/adnen/OneDrive/Documents/20250108_165104.bag")
# Parse the command line arguments to an object
args = parser.parse_args()
# Safety if no parameter have been given
try:
# Create pipeline
#align_to = rs.stream.color
#align = rs.align(align_to)
pipeline = rs.pipeline()
# Create a config object
config= rs.config()
# Tell config that we will use a recorded device from file to be used by the pipeline through playback.
rs.config.enable_device_from_file(config, "C:/Users/adnen/OneDrive/Documents/20250108_165104.bag")
#config.enable_stream(rs.stream.depth, 640, 480, rs.format.z16, 30)
temporal_filter = rs.temporal_filter()
spatial_filter = rs.spatial_filter()
temporal_smooth_alpha = 0.63
temporal_smooth_delta = 55
persistency_index = 8
temporal_filter.set_option(rs.option.filter_smooth_alpha, temporal_smooth_alpha)
temporal_filter.set_option(rs.option.filter_smooth_delta, temporal_smooth_delta)
temporal_filter.set_option(rs.option.holes_fill, persistency_index)
profile = config.resolve(pipeline)
# Start streaming from file
pipeline.start(config)
# Create opencv window to render image in
cv2.namedWindow("Depth Stream", cv2.WINDOW_AUTOSIZE)
cv2.setMouseCallback("Depth Stream", mouse_callback)
# Create colorizer object
colorizer = rs.colorizer()
colorizer.set_option(rs.option.min_distance,2.1)
colorizer.set_option(rs.option.max_distance,3.3)
colorizer.set_option(rs.option.color_scheme,4)
# Streaming loop
while True:
# Get frameset of depth
frames = pipeline.wait_for_frames()
# Get depth frame
depth_frame = frames.get_depth_frame()
color_frame = frames.get_color_frame()
#aligned_frames = align.process(frames)
#color_frame = aligned_frames.get_color_frame()
#depth_frame = aligned_frames.get_depth_frame()
depth_intrinsics = depth_frame.profile.as_video_stream_profile().intrinsics
# Get the color frame intrinsics
color_intrinsics = color_frame.profile.as_video_stream_profile().intrinsics
color_image = np.asanyarray(color_frame.get_data())
depth_frame = temporal_filter.process(depth_frame)
# Colorize depth frame to jet colormap
depth_color_frame = colorizer.colorize(depth_frame)
#depth_frame = hole_filling_filter.process(depth_frame)
depth_data = np.asanyarray(depth_frame.get_data())
# Convert depth_frame to numpy array to render image in opencv
depth_color_image = np.asanyarray(depth_color_frame.get_data())
# Convert the image to HSV color space
hsv = cv2.cvtColor(depth_color_image, cv2.COLOR_BGR2HSV)
# Define the range for the greenish color
lower_green = np.array([35, 50, 50]) # Adjust these values based on the green shade
upper_green = np.array([85, 255, 255]) # Adjust these values based on the green shade
# Create a mask for the green color
mask = cv2.inRange(hsv, lower_green, upper_green)
# Apply the mask to the original image
depth_color_image = cv2.bitwise_and(depth_color_image, depth_color_image, mask=mask)
contours, _ = cv2.findContours(mask, cv2.RETR_EXTERNAL, cv2.CHAIN_APPROX_SIMPLE)
if contours:
# Find the largest contour (assuming the green shape is the largest green object)
largest_contour = max(contours, key=cv2.contourArea)
# Approximate the contour to a polygon
epsilon = 0.02 * cv2.arcLength(largest_contour, True)
approx = cv2.approxPolyDP(largest_contour, epsilon, True)
# Check if the approximated contour has 4 points (rectangle)
if len(approx) == 4:
rectangle_points = approx.reshape(4,2)
reordered_points = reorder_rectangle_points(rectangle_points)
rectangle_points=reordered_points
p1 = rectangle_points[0]
p2 = rectangle_points[1]
p3 = rectangle_points[2]
p4 = rectangle_points[3]
depth1 = depth_data[p1[1], p1[0]] * 0.00025 # (y, x) order for depth frame
depth2 = depth_data[p2[1], p2[0]] * 0.00025
depth3 = depth_data[p3[1], p3[0]] * 0.00025
depth4 = depth_data[p4[1], p4[0]] * 0.00025
print(depth1)
point1c = rs.rs2_deproject_pixel_to_point(depth_intrinsics, [p1[0], p1[1]], depth1*1000)
point2c = rs.rs2_deproject_pixel_to_point(depth_intrinsics, [p2[0], p2[1]], depth2*1000)
point3c = rs.rs2_deproject_pixel_to_point(depth_intrinsics, [p3[0], p3[1]], depth3*1000)
point4c = rs.rs2_deproject_pixel_to_point(depth_intrinsics, [p4[0], p4[1]], depth4*1000)
distance1 = math.sqrt((point2c[0] - point1c[0])**2 +(point2c[1] - point1c[1])**2 + (point2c[2] - point1c[2])**2)
distance2 = math.sqrt((point3c[0] - point2c[0])**2 +(point3c[1] - point2c[1])**2 + (point3c[2] - point2c[2])**2)
distance3 = math.sqrt((point4c[0] - point3c[0])**2 +(point4c[1] - point3c[1])**2 + (point4c[2] - point3c[2])**2)
distance4 = math.sqrt((point4c[0] - point1c[0])**2 +(point4c[1] - point1c[1])**2 + (point4c[2] - point1c[2])**2)
#color_image=cv2.resize(color_image,(680,420),cv2.INTER_AREA)
p1x=rs.rs2_project_point_to_pixel(color_intrinsics, point1c)
p2x=rs.rs2_project_point_to_pixel(color_intrinsics, point2c)
p3x=rs.rs2_project_point_to_pixel(color_intrinsics, point3c)
p4x=rs.rs2_project_point_to_pixel(color_intrinsics, point4c)
print(p1x)
print([p1[0], p1[1]])
p1x[1]=+45
p1x[0]=int(p1x[0])-10
p2x[0]=int(p2x[0]) -10
p2x[1]=int(p2x[1]) +36
p3x[0]=int(p3x[0])-10
p3x[1]=int(p3x[1])+ +36
p4x[0]=int(p4x[0])-10
p4x[1]=int(p4x[1])+36
#print(p2x)
#print(p3x)
#print(p4x)
# Draw arrows and distances
depth_color_image=color_image
draw_distance_with_arrows(depth_color_image, p1x, p2x, f"{distance1:.3f} mm", (0, 0, 255)) # Green arrow for distance1
draw_distance_with_arrows(depth_color_image, p2x, p3x, f"{distance2:.3f} mm", (255, 0, 0)) # Blue arrow for distance2
draw_distance_with_arrows(depth_color_image, p3x, p4x, f"{distance3:.3f} mm", (0, 255, 255)) # Yellow arrow for distance3
draw_distance_with_arrows(depth_color_image, p4x, p1x, f"{distance4:.3f} mm", (255, 255, 0)) # Cyan arrow for distance4
# Calculate angles at each corner
angle1 = calculate_angle(point4c,point1c, point2c)
angle2 = calculate_angle(point1c, point2c, point3c)
angle3 = calculate_angle(point2c, point3c, point4c)
angle4 = calculate_angle(point3c, point4c, point1c)
# Draw angles on the image
draw_angle(depth_color_image, p4x, p1x, p2x, angle1, (0, 0, 255),False) # Red
draw_angle(depth_color_image, p1x, p2x, p3x, angle2, (0, 255, 255),True) # Green
draw_angle(depth_color_image, p2x, p3x, p4x, angle3, (255, 0, 0),False) # Blue
draw_angle(depth_color_image, p3x, p4x, p1x, angle4, (255, 255, 0),False) # Yellow
# Draw the rectangle points on the original image
for f,point in enumerate(rectangle_points):
if f==0 :
cv2.circle(depth_color_image, tuple(p1x), 10, (0, 0, 255), -1) # red points
if f==1 :
cv2.circle(depth_color_image, tuple(p2x), 10, (255, 0, 0), -1) # blue points
if f==2 :
cv2.circle(depth_color_image, tuple(p3x), 10, (0, 255, 255), -1) # yellow points
if f==3 :
cv2.circle(depth_color_image, tuple(p4x), 10, (255, 255, 0), -1) # purple points
#Draw the contour
#cv2.drawContours(depth_color_image, [approx], -1, (0, 0, 255), 2) # Red contour
else:
print("The shape is not a rectangle.")
cv2.imshow("Depth Stream", depth_color_image)
#cv2.imshow("Depth Stream", depth_color_image)
key = cv2.waitKey(1)
# if pressed escape exit program
if key == 27:
cv2.destroyAllWindows()
break
finally:
pass
-
Hi Adnentrimech123,
Thanks for reaching out to Intel® RealSense™ Technical Support.
To align depth frame pixel to image frame pixel, please refer to align-depth2color.py in Sample Code for Intel® RealSense™ Python Wrapper and modify your existing code.
Regards,
Wai Fook
Intel Customer Support
Please sign in to leave a comment.
Comments
1 comment