L515 Unable to update firmware
On a new L515 unit I received, when I try to update the firmware to 1.5.3 using either the command line or the tool in RealSense Viewer, I get this error:
"firmware update progress: 8[%]RealSense error calling rs2_update_firmware_cpp(device:000001AE9E6F7800, fw_image:000001AE9F1E4060):
Device: 0003ac7ee5cd failed to download firmware
Please verify that no other librealsense application is running"
I don't have any other instances of RealSense running. And I have tried downloading the FW directly from the Intel website, but I get the same error.
Can anyone help?
-
Hello Jon,
Please tell us more about your environment.
- Does the L515 work correctly with RealSense Viewer, i.e. are you able to see both Depth and RGB streams?
- Which version of the RealSense SDK are you using?
- Did you install the SDK by building from source or from binaries?
- Which OS are you using?
- Are you using the USB cable that came with the camera?
- Is the L515 being recognized as a USB 3 device or USB2?
- Have you tried to update the firmware using different computers?
Sincerely,
Jesus G.
Intel Customer Support
Please sign in to leave a comment.
Comments
3 comments