RealSense Support

D455 configuration, saving, recording

Comments

1 comment

  • MartyX Grover

    Hi Jimmek  Yes, the json save / load buttons near the top of the RealSense Viewer's options side-panel can export settings under the Stereo Module section (Including Advanced Mode) to a json file that can be re-imported.

     

     

    The RGB and Motion Module functions are not supported in the entire range of RealSense 400 Series models.  All the cased models have RGB but only D435i and D455 cased models have an IMU.  On the caseless Depth Module Kit circuit-board versions of the cameras, only the D415 board has an RGB sensor).

    The Stereo Module options are supported on all 400 Series models though. 

     

    Command-line recording of an SDK bag file is available in the rs-record tool.

    https://github.com/IntelRealSense/librealsense/tree/master/tools/recorder 

    0
    Comment actions Permalink

Please sign in to leave a comment.