RealSense Support

How to convert the ROS Image obtained from the L525 Lidar camera to real world units

Comments

9 comments

  • Rizal Marzuki

    Hi Kashish Dhal,

    Why am I getting 8 bit depth image? Shouldn't it be 16 bit?
    You are splitting the 16 bit to two matrix.
    I would suggest you look at the typecast and swapbytes functions.
    Try to checking out this discussion about merging two 8 bit to 16 bit.

    Why am I getting 480x640 pixels? 
    You are getting that resolution because it is the resolution you recorded (it is the default resolution for depth camera)

    Secondly, how do I convert the value of the pixels from the 0-255 to meters.
    You would need to multiply the 16bit value with the the depth camera and add the offset.

    The topic should be similar to:

    • /device_0/sensor_0/option/Depth_Units/value    for conversion (it is in meters)
    • /device_0/sensor_0/option/Depth_Offset/value    for offset (it is in milimeters)

    Note: Check your topics. In my case, the depth camera was sensor_0. 

    You could try something similar to the following:

    X = swapbytes( [Dxy Cxy] );
    Depth(x,y) = double( typecast(X,'uint16') * depth_units )  + (offset / 1000) ;

    Regards,
    Rizal

     

    0
    Comment actions Permalink
  • Kashish Dhal

    Hello Rizal,

    Thank you very much for the reply!

    So, I am not splitting the depth image into 2 matrix, but actually from ROS side, I am getting the data as a vector of size 614400. Now this fits into two matrices of 640x480. So I was forced to do so.

    Just before getting your reply, I figured that they should be combined to make one matrix. So this is what I did:

    imgD = reshape(imgData(1:2:end),imgW,imgH)';
    imgC = reshape(imgData(2:2:end),imgW,imgH)';

    imgCombined = imgCx2^8 + imgD;

    This operation is equivalent of what you suggested, typecasting the uint8_t to uint16_t and then swapping the two bytes. But can you suggest something that takes a vector of length 614400 as input and outputs a 640x480 matrix. I am doing this in 3 lines of code as above, if you can suggest something that can be done in one line it will be great!

    If I am getting the default resolution then it is fine!

    The following you are referring to are ROS topics?

    • /device_0/sensor_0/option/Depth_Units/value    for conversion (it is in meters)
    • /device_0/sensor_0/option/Depth_Offset/value    for offset (it is in milimeters)

    Currently, I have calibrated the camera myself by taking the distance measurements at different position from camera:

     

    Regards,

    Kashish Dhal

     

    0
    Comment actions Permalink
  • Rizal Marzuki

    Hi Kashish Dhal,

    The following you are referring to are ROS topics?

    Yes, you would need those values from the topics for the following equation.

    result = (imgCombined * Depth_Units_value)+ (Depth_Offset_value/1000)

    It should get you the depth in meters..

    Regards,
    Rizal

    0
    Comment actions Permalink
  • Kashish Dhal

    Hello Rizal,

    Thanks for the reply!

    Unfortunately, I can't see the topics that you have mentioned, see below:

     

    gnclab@system76-pc:~$ rostopic list
    /camera/depth/camera_info
    /camera/depth/image_rect_raw
    /camera/depth/image_rect_raw/compressed
    /camera/depth/image_rect_raw/compressed/parameter_descriptions
    /camera/depth/image_rect_raw/compressed/parameter_updates
    /camera/depth/image_rect_raw/compressedDepth
    /camera/depth/image_rect_raw/compressedDepth/parameter_descriptions
    /camera/depth/image_rect_raw/compressedDepth/parameter_updates
    /camera/depth/image_rect_raw/theora
    /camera/depth/image_rect_raw/theora/parameter_descriptions
    /camera/depth/image_rect_raw/theora/parameter_updates
    /camera/infra/camera_info
    /camera/infra/image_raw
    /camera/infra/image_raw/compressed
    /camera/infra/image_raw/compressed/parameter_descriptions
    /camera/infra/image_raw/compressed/parameter_updates
    /camera/infra/image_raw/compressedDepth
    /camera/infra/image_raw/compressedDepth/parameter_descriptions
    /camera/infra/image_raw/compressedDepth/parameter_updates
    /camera/infra/image_raw/theora
    /camera/infra/image_raw/theora/parameter_descriptions
    /camera/infra/image_raw/theora/parameter_updates
    /camera/l500_depth_sensor/parameter_descriptions
    /camera/l500_depth_sensor/parameter_updates
    /camera/motion_module/parameter_descriptions
    /camera/motion_module/parameter_updates
    /camera/realsense2_camera_manager/bond
    /camera/rgb_camera/parameter_descriptions
    /camera/rgb_camera/parameter_updates
    /diagnostics
    /rosout
    /rosout_agg
    /tf
    /tf_static

    Also, I wanted to convert the long vector of size 614400 into the 640x480 vector in C++. Would you suggest some efficient way of doing that? Should I use two nested for loops or something else?

    0
    Comment actions Permalink
  • Rizal Marzuki

    Hi Kashish Dhal,

     

    My mistake, I was inspecting rosbag from RealSenseViewer recording.

    Can you try checking the content of /camera/depth/camera_info topic?

     

    Regards,

    Rizal

    0
    Comment actions Permalink
  • Kashish Dhal

    Hello Rizal,

     

    I am getting the following message:

    gnclab@system76-pc:~$ rostopic echo -n1 /camera/depth/camera_info
    header: 
      seq: 519
      stamp: 
        secs: 1605317106
        nsecs: 955127954
      frame_id: "camera_depth_optical_frame"
    height: 480
    width: 640
    distortion_model: "plumb_bob"
    D: [0.0, 0.0, 0.0, 0.0, 0.0]
    K: [459.37890625, 0.0, 334.30078125, 0.0, 460.34375, 248.58984375, 0.0, 0.0, 1.0]
    R: [1.0, 0.0, 0.0, 0.0, 1.0, 0.0, 0.0, 0.0, 1.0]
    P: [459.37890625, 0.0, 334.30078125, 0.0, 0.0, 460.34375, 248.58984375, 0.0, 0.0, 0.0, 1.0, 0.0]
    binning_x: 0
    binning_y: 0
    roi: 
      x_offset: 0
      y_offset: 0
      height: 0
      width: 0
      do_rectify: False
    ---
    
    0
    Comment actions Permalink
  • Rizal Marzuki

    Hi Kashish Dhal,

     

    If you have not adjusted your L515, even with differing presets the values obtained  are:

    depth unit is 0.00025 meter

    and the offset is 4.5 millimeter

     

    Regards,

    Rizal

    0
    Comment actions Permalink
  • Kashish Dhal

    Hello Rizal,

     

    Are you giving me the default values? or are you reading it from the rostopic? If yes, how?

    0
    Comment actions Permalink
  • Harleyzheng

    Hi guys

    Can someone explain what this line of code is doing and how to use it?:

    imgCombined = imgCx2^8 + imgD;

    When i use it I get: Unrecognized function or variable 'imgCx2'.

    Cheers

    0
    Comment actions Permalink

Please sign in to leave a comment.