I can connect D435i to PC via wireless or WIFI ?
I can connect D435i to pc via wireless or WIFI?
Does it only connect by USE?
-
Hi Minolta Vet An option for wireless communication may be to take control of the computer or computing device that the camera is attached to from another location using remote connection software. An example of this is Chrome Remote Desktop which allows connection of computer to computer or phone / tablet to computer.
https://remotedesktop.google.com/?pli=1
There was also a case where a RealSense user put a RealSense device on a drone and connected to the drone's on-board computer via wi-fi.
https://github.com/IntelRealSense/librealsense/issues/4392
In regard to physical cabling alternatives to USB, you can use CAT5 ethernet cabling and access a camera as a Network Device via an IP address, though the data transfer speeds achievable on ethernet will be lower than on USB. Intel have published a white-paper document on open-source ethernet networking with RealSense.
Please sign in to leave a comment.
Comments
1 comment