SR300 IR Stream Performance
Hello,
I took IF stream by using SR300 camera. In some circumstance, IF stream has lighted area as seen on first image. As far as I know, IF stream shouldn't have this kind of light and dark areas. Could you help me to get rid of these kind of situation? You can see the desired image version taken from IF stream in the second picture, which doesnt have any transmission.


-
The difference between one image and another seems reasonable, considering that:
- There is a reflective glass window inbetween the camera's apparent position and the observed person behind the window
- It is an outdoor scene with variable natural lighting
If it is confirmed that glare from window reflections is the source of the differences then you may be able to significantly reduce the effect on the camera image of such glare by applying a physical optical filter called a linear polarizer over the camera lens. Section 4.4 of Intel's white-paper document about optical filters provides a lot of detail about this subject.
Please sign in to leave a comment.
Comments
1 comment