RealSense Support

What is the difference between Image Sensor Technology and RGB Sensor Technology?

Comments

1 comment

  • MartyX Grover

    Hi Roni Dem  There are additional differences between the D435i and D455 that improve depth to color alignment.  The D455 color and depth imagers have the same FOV size (the D435 models have a larger depth FOV than color).  The color and depth imagers are mounted on the same stiffener inside the camera, resulting in improved alignment between color and depth. 

    Also, the D455 has 2x the accuracy over distance of the D435 models, so the D455 has the same accuracy at 6 meters that the D435 models have at 3 meters.

    The changes are summarized in the Intel press release in the link below:

    https://newsroom.intel.com/news/intel-realsense-depth-camera-d455-twice-range-better-performance/#gs.hh1v7z 

    0
    Comment actions Permalink

Please sign in to leave a comment.