RealSense Support

Humid environment - enclosure L515 sensor

Comments

1 comment

  • Official comment
    Jesus Garcia

    Hello Erwin,

    Intel does not recommend to place the L515 in a fully enclosed housing because that would require the placement of a transparent material in front of the camera, which would degrade performance. There should be no other glass or plastic of any kind between the L515 and the target object/scene because it would interfere with the projected and reflected lasers.

    Section 4.5 of the Intel RealSense L515 datasheet states the supported operating conditions of the camera. Any custom housing you design should meet the listed constraints and avoid placing any material in front of the camera.

    Additionally, opening the chassis of the L515 is not supported and voids the warranty.

    Sincerely,
    Jesus G.
    Intel Customer Support

    Comment actions Permalink

Please sign in to leave a comment.