View my account

D435i , failed to display

Comments

10 comments

  • MartyX Grover

    Hi Patrick Yu C W  Does the image also disappear in 2D mode or only in 3D point cloud mode?

    Also, does the depth still disappear in 3D mode if you only have Depth enabled?

    0
    Comment actions Permalink
  • Patrick Yu C W

    Even in Depth enabled mode still have same problem. Results are as follows :

    0
    Comment actions Permalink
  • MartyG

    There was a similar sounding problem reported recently where the depth image in 3D point cloud mode in the Viewer was disappearing after 3-4 seconds.

    https://github.com/IntelRealSense/librealsense/issues/8110 

    The solution in that particular case was to disable GLSL in the Viewer's settings.

    https://github.com/IntelRealSense/librealsense/issues/8110#issuecomment-754705023 

    0
    Comment actions Permalink
  • Patrick Yu C W

    Problem fixed ! But cannot disable both GLSL feature, else the "measure" function will be disabled also !

    Another issue, for the below picture, the Door (in red box) is only 5 meters apart from the CAM but cannot shown and measure. What is the effective detective and measurable distance for D435i ?

    Thanks !

    0
    Comment actions Permalink
  • MartyG

    The measurement function is available in a separate tool via the rs-measure program if you are unable to access it within the 3D mode of the Viewer when GLSL is disabled.

    https://github.com/IntelRealSense/librealsense/tree/master/examples/measure 

    If the door is 5 meters away and not rendered on the depth image, please expand open the Post processing options that are within the Stereo Module options in the side-panel.  Within the list of post processing filters, find one called Threshold Filter.  

    The purpose of this filter is to define a minimum and maximum observable depth, with data outside of the defined range excluded from the image.  It is set to 4 (meters) by default.  If it is enabled (indicated by a blue icon beside it), increase the setting's value to render further depth distance or left-click on the blue icon to toggle it to Off to remove the 4 meter rendering limitation.

    0
    Comment actions Permalink
  • Patrick Yu C W

    My Realsense disappear again and the photo is keep still not following the camera

    0
    Comment actions Permalink
  • MartyX Grover

    There was a similar case on the RealSense GitHub forum in the past week of the image disappearing in 3D mode.  The solution though was to disable GLSL in the settings, which you have previously stated is a problem for you due to losing access to the Measure function of the Viewer when doing so.

    https://github.com/IntelRealSense/librealsense/issues/8813

    Does the image disappear if you disable Use GLSL for Processing but keep Use GLSL for Rendering enabled in order to keep the Measure option accessible?

     

    0
    Comment actions Permalink
  • Patrick Yu C W

    It still disappear in 3D view but It 's ok in 2D view

    0
    Comment actions Permalink
  • MartyX Grover

    I will highlight your case and the GitHub one to Intel.  There is no other corrective advice that I can suggest at present though other than to disable both GLSL options at the cost of lack of access to the Measure function if you need to use the 3D mode.

    0
    Comment actions Permalink
  • Patrick Yu C W

    Thank you MartyG ! Looking forward to the solution .

    0
    Comment actions Permalink

Please sign in to leave a comment.