RealSense Support

high resolution 3d face scan

Comments

3 comments

  • MartyX Grover

    Hi Francois Lessard Ciussse-chus  The D415 would be highly suitable for your needs.  Its optimal-accuracy depth resolution is 1280x720 and it is well suited to scanning static or slow-moving objects.  The D415 can also operate very effectively in a wide range of indoor and outdoor environmental conditions and lighting.

    0
    Comment actions Permalink
  • Francois Lessard Ciussse-chus

    Thanks for the quick answer. Which depth delta should I be able to measure with either D415 and L515 in controlled indoor lighting conditions?

    0
    Comment actions Permalink
  • MartyX Grover

    I am not involved in technical support for the L515 model.  Please create a separate case on this forum for that particular question and set it to the 'L515' topic name.  Thanks!

    0
    Comment actions Permalink

Please sign in to leave a comment.