Error when installing the realense UWP SDK
I have this problem.
I installed it on another computer just in case.
have the same symptoms
install error : There was a problem adding drivers to the repository.

-
Hi Kweon9612 You do not need to have the UWP driver installed in order to use RealSense with Windows. The driver provides an interface between RealSense and products that support Microsoft's Universal Windows Platform (UWP), such as the Hololens headset. So most RealSense users do not need to have the driver installed.
-
HI MartyG
I want to run Realesne as UWP using Unity3D.
However, the webcam will run, but D435 will not.
I wonder if this has anything to do with the UWP SDK. -
The latest version of the UWP driver at the time of writing this (6.11.160.21) may cause errors in Unity.
https://github.com/IntelRealSense/librealsense/issues/7425
If you need to use UWP, it is recommended to use the earlier version of the driver.
Please sign in to leave a comment.
Comments
3 comments